Please choose your delivery location

The selection of the country/region page can influence various factors such as price, shipping options and product availability.

Cables resistant to the elements

Heavy duty application overhaul

This large RMG crane is exposed to over 300 days of sunshine per year. this retrofit included CFLG cables and cables with TPE jacketing due to the environmental concerns. 
This crane had design issues causing significant downtime
Fiber optic cables play an important role in avoiding crane downtime. FOC are vital in maintining communication with the various sensors and data equipment. 

chainflex cables are designed to increase overall durability in maritime environments. TPE jacketing  has increased UV resistance to extend trolley hours.

igus cables and chains have an average life expectancy between 15,000-25,000 trolley hours based on chain series. That's an average lifespan of up to 10 years! 
Complete replacement designed for maritime environment

chainflex® cables on ship loader

This ship loader was retrofitted to handle various bulk materials. It can handle 720 tons per hour. Several different types of bulk materials are handled. Speed: 1.1 ft/s (0.3 m/s) , Travel distance: 639.8 ft (195 m)

The motor, bus and control cables - specifically  Siemens SPS7 programmable logic controller to control the entire facility - were routed through a E4/4 type, Series 5050 cable carrier.

Potential inductive interference fields that could affect the signal transmission were prevented by a special shielding on the bus and control cables. All the power and control cables used inside the cable carrier come from the chainflex® continuous-flex cable range from igus®.

Since the ship loader started operating over ten years ago, there have been no reported problems with the cable carrier system. None of the cables or cable carrier links have had to be replaced.
Series 5050 cable carrier, center mounted in stainless steel guide trough

More on applied products here:

More applications from different industries can be found here

Useful Links

Browse Additional Cables

Hybrid Cables

Hybrid Cable
Hybrid cables combine servo & motor feedback cables for drive technology & are becoming the norm for use in servo drive systems.  The fast, precise movements required benefit from having just a single cable relaying the necessary energy & signals.  Learn more here.
 
Browse the Shop

readycable® Cable Assemblies

readycable
Our line of motor, servo, signal and encoder cable assemblies comes equipped with standard industrial connectors that are ready to connect to your application.  All of our cable assemblies are built similar to 24 manufacturer’s standards such as Siemens, Allen Bradley & Beckhoff.  Learn more here.
 
Browse the Shop

Request a Free Sample Box

chainflex sample box Simply fill out the form below and we will ship you a free sample box.
Request a free sample box

Request or Download the Catalog

chainflex catalog Click below to request a catalog or view the PDF version.
Request a Catalog

Contact an ECS Expert

Contact Stephen Shukur Contact ECS expert Stephen Shukur for flexible cables and plastic cable carriers related to ports, intermodal, and container handling industries.
Contact an expert

Contact an ECS Expert

Dave Kortkamp

Contact an ECS expert Dave Kortkamp for flexible cables and plastic cable carriers related to ports, intermodal, and container handling industries.

Contact an expert



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® SE & Co. KG

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302